尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。

The new Liquiphant FTL51 - The pioneer

Once the first vibronic point level detector, the Liquiphant is now ready for Industry 4.0

发行日期: 30.09.2019

Digital change

Whether as overfill protection or dry run protection, the Liquiphant today performs many tasks in the automation of processes. But even the most simple measuring principles have to adapt to digital change. It was time to equip the sensor for the tasks of tomorrow. Those who prepare their company for the digital age today will optimize their field level as well as their information technology. This requires sensors that provide relevant data in order to initiate process optimization.

Process sensors 4.0

In the technology roadmap to „Process sensors 4.0“ NAMUR demands that a second, mobile way to communicate with the sensor must be opened and that the sensor provides information for preventive maintenance and process optimization. Furthermore product information such as manuals or certificates must be available on site at all times. Operators can now communicate with the Liquiphant and the SmartBlue App from Endress+Hauser. The app provides access to all product and diagnostic data.

The new generation

Especially in hard-to-reach areas, where scaffolding has to be provided for maintenance, this speeds up the inspection of systems considerably. The new Liquiphant displays the status of the level switch via LED or via the diagnostic function of Heartbeat Technology in the SmartBlue App. In addition verification via Heartbeat Technology enables complete documentation. The newly implemented SIL Wizard also guides the user through the recurring test in an uncomplicated manner.

Simplicity and Safety

All the digital innovations of the new generation of devices serve only the purpose of simplifying human work. The The Liquiphant is used in storage tanks and pipelines for level measurement of any liquids. The all-rounder also works where other measuring principles reach their limits due to conductivity, flows or air bubbles. The Liquiphant has already been developed according to IEC 61508 and the "Safety by Design" principle and is therefore designed for use in SIL2 and SIL3 applications.

新闻列表

通过邮箱直接接收下一条新闻稿和新闻。订阅Endress+Hauser新闻列表,时刻关注最新动态。

Endress+Hauser press list

Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

Select the topics you are interested in:  *
Select the industries you are interested in: *

Personal Data


Fields marked with * are required. You will receive an email with a confirmation of your subscription. The information enlisted is voluntary and your data will only be used for personalizing your newsletters and not be passed onto any third party. For statistical reasons we will perform anonymous link tracking.