Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
Lịch sử
Optimized diagnostics and maintenance: Smart Support Connect
Wastewater treatment plants are testing the CA80 analyzer with cloud-based support platform
The introduction of the new Smart Support Connect service minimizes manual work and reduces the time and cost of operating and maintaining wet-chemical analyzers for customers in wastewater treatment plants. Within this context, Endress+Hauser is working with various companies in the wastewater sector, for example, the Emschergenossenschaft/Lippenverband (EGLV) wastewater management company in Germany and the Municipality of Kincardine in Canada.
Remote support for the customer on site via the Endress+Hauser support platform using live video transmission tool
Measuring station for aeration basin with CA80PH orthophosphate analyzer
The results
Cost and time savings
Transfer of knowledge
Fault-free operation guaranteed
Endress+Hauser is developing a proactive, web-based servicing and maintenance tool in line with the principles of "Industry 4.0" to minimize the effort associated with maintenance and repair work.
Dirk Desinger, Technical Services business division
wastewater department, Emschergenossenschaft/Lippenverband (EGLV)
More services should go in this direction.
Shamus Anderson
Municipality of Kincardine
Customer challenge
Diagnosing and remedying faults on the analyzer of wastewater treatment plants can be very complex, as many plants are located in rural areas and extensive expertise is often required.
Our solution
As part of a joint «Water management 4.0» project, Endress+Hauser developed a measuring station for sample filtration comprising a CA80PH orthophosphate analyzer and CAT820 sample preparation system. An edge device was used to connect it to the Endress+Hauser Netilion IIoT platform over the mobile network for remote support.
In order to minimize the effort associated with maintenance and repair work, Emschergenossenschaft/Lippenverband (EGLV) in Germany collaborated with Endress+Hauser to install a measuring station for their aeration basin.
Chúng tôi sử dụng cookie để nâng cao trải nghiệm duyệt web của bạn, thu thập số liệu thống kê để tối ưu hóa chức năng của trang web và cung cấp nội dung hoặc quảng cáo phù hợp.
Bằng cách chọn "Chấp nhận tất cả", bạn đồng ý với việc sử dụng cookie của chúng tôi.
Để biết thêm chi tiết, vui lòng xem lại Chính sách cookie của chúng tôi.