Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
  • Lịch sử

Monitoring surface water

Netilion Smart System in the municipality of Baltschieder

The municipality of Baltschieder uses the new Netilion Smart System to reliably and continuously record the pH, conductivity, turbidity and temperature of the River Baltschieder surface water. This enables a digital analysis of the values to ensure that any contamination in the river are detected and tracked.

River Baltschieder

Measuring water quality in the River Baltschieder

Liquiline transmitter

Liquiline transmitter

Results

  • Continuous monitoring of water quality

  • Measured values displayed via the Netilion Smart Systems smartphone App

  • Trend indicator on smartphone for previous 24 hours

  • Diagnostic information relating to instrument status

  • Data export to Excel for analysis and documentation

Philipp Kalbermatten

"The measured values are continuously transmitted to the Netilion Cloud and can be called up easily from a workstation"

Philipp Kalbermatten
Municipality of Baltschieder

The challenge

Up until now, the municipality of Baltschieder has not had access to consistent information on certain parameters relating to the water quality of the River Baltschieder. This meant that contamination or natural effects were not detected and dealt with in a timely manner.

What was needed was a reliable monitoring system that required little effort to install and maintain.

Solution

The Netilion Smart System for surface water ensures reliable detection of the water quality parameters required by the municipality:

  • Turbidity: The smart Turbimax CUS52D sensor measures turbidity and enables low-maintenance operation.

  • Conductivity: The Condumax CLS21D is a robust and accurate conductivity sensor for all process and environmental applications.

  • pH: The Orbisint CPS11D is a durable and digital all-round technology. It provides reliable measurements and requires little maintenance.

These water quality measurements are collected by the multi-channel Liquiline CM444. The Modbus Edge Device transmits the measured data to the Netilion Cloud. These measurements are easily and remotely accessible via the Netilion Smart System App. Furthermore, the smartphone application also offers diagnostic and alarm information directly into the hands of the customer.

Components

This Netilion Smart System includes:

  • Turbimax CUS52D sensor

  • Condumax CLS21D sensor

  • Orbisint CPS11D sensor

  • Liquiline CM444 transmitter

  • Modbus Edge Device

  • Netilion Smart Systems App